MLG-2 WebChecker - measuring thick objects - part 2
Related Products
Table of Contents
In my last blog, I told you about the restrictions we have with thick objects.
Here, I want to show you how to handle thick objects with full measurement performance.
Circular Objects
tubes, pipes, rods, balls
Example for circular tube:
Measuring the diameter of round tubes, even when thicker than specified in our instruction manual.
Due to the curved edges, we can measure the diameter precisely.
Condition: the center of the tube must remain in the 1/3 – 2/3 section.
Result:
Both edges can be measured with full performance.
Position & width → with full resolution and high precision.
Right angle objects
plates or lying round parts
Example for a right angle box
In that case we can tilt the sender – receiver, so that we can measure one edge precisely (alternatively the box can be tilt).
Attention: we only can reach a valid measurement for the upper edge - due to the angle of the crossed beam.
Of course, the measured edge must be positioned according to the 1/3 - 2/3 rule.
As you can see at the bottom edge, we get invalid measurement due to the beam shadow at the back side of the box.
No width measurement!
Example for a hanging wheel rim
In that example we can measure precisely the height of the wheel rim.
FAQ
- Is width measurement less accurate then single edge measurement?
Almost not. - What tilt angle is needed for the position measurement of wheel rim in the example above?
A small angle around 1…3° is enough due to the slight beam angle of crossed beams. - How many tubes can be measured side by side?
max. 5 – due to 10 edges - How to configure width measurement via SOPAS?
Function Configuration → allocating F1, F2, etc - What can happen when the No. of tubes changes during process?
the numeration of edges will change → loss of width measurement for the allocated functions - How to solve that?
You can solve this using search fields.
webchecker, measuring thick objects, circular objects, right-angled objects