web
You’re offline. This is a read only version of the page.
close
Support Portal

Is the metal shaft collet with a diameter of 1/4" for the DUS60 also available as a spare part and in plastic?

Is the metal shaft collet with a diameter of 1/4" for the DUS60 also available as a spare part and in plastic?
Related Products
incremental encoders
DUS60

Table of Contents

If you check the product family overview of the DUS60 you will notice that there is also an hollow shaft diameter of 1/4" available.

Unlike the other diameters, there is NO metal shaft collet nor a plastic shaft collet as a spare part for this diameter available.

This hollow shaft with a diameter of 1/4" is only available when installed in the encoder.

Keywords:
DUS60, hollow shaft, encoder, shaft collet, diamter 1/4"