web
You’re offline. This is a read only version of the page.
close
Support Portal

SRM50-HZV0-S24 (1053906); SRS50-HZV0-S24 (1053907) special encoder

Table of Contents

The encoders ...

  • SRM50-HZV0-S24 (1053906)
  • SRS50-HZV0-S24 (1053907)

... are special encoders with the following attributes:

  • 1024 SIN/COS periods per revolution
  • Absolute position with 15 bit per revolution (32'768 steps)
  • customer specific stator coupling (CT / control techiques) -> see picture
  • It is no more sellable
  • There is no suitable replacement, please contact the motor supplier,
  • The SRM50-HZV0-S24 (1053906) was the replacement for the SRM50-HZV0-S01 (1034152)
  • The SRS50-HZV0-S24 (1053907) was the replacement for the SRS50-HZV0-S01 (1034212)

see also the picture and the attached data sheets

Keywords:
srs50, srm50, hiperface, special, customized, encoder, motor feedback