Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
What is the difference between the NAV210 and the NAV245
The NAV210 is giving out contour measurements with a high angular accuracy for contour localization. The NAV245 can additionally detect precisely reflector coordinates and provides these coordinates including a timestamp for an external reflector based localization.
How can I retrieve the angular data from the NAV210 and NAV245 and how to process it ?
To read out the compensation table please use this command:
Is is possible to retrieve the RDI ( Reflector Data Inferface ) information from the NAV245 via RS232 ?
Yes, it is possible to use the command the sSN NLMDLandmarks via RS232. For a permanent output of the RDI data it is necessary to avoid the output of contour data.
For real time time transmission of contour data (plus RDI data ) the RS232 interface is not suitable.
How to reset the NAV2xx by a telegram?
Der NAVxxx is supporting these commands, which are available in the userlevel "Authorized clientï"
sMN mSCreboot
( Method executes a software reset on the device )
and
sMN mSCsoftreset 0
( Method shuts the device down but saves the parameter before shutdown is executed )
The first method executes only a reset, while the second method will save the current parameter before executing the reset.