Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
The STL70 / ETL70 is a kit system. The measuring unit and the measuring scale are sold independent.
The information about the STL70 / ETL70 accuracy is only about the sensor. For the overall accuracy, we also have to take the magnetisation accuracy of the magnetic tape into account.
There it is important to know, that the system is a positioning system. The repeatability is very high (< 1 µm). But if you want to measure a distance, you have to add some accuracy values.
How is the accuracy calculated?
Which values do we have?
accuracy read head: 10 µm
accuracy measuring tape each meter: 30 µm
Depending on the length of the system, you take for each meter the accuracy value 30 µm + one time the accuracy of the read head (10 µm).
This means, the accuracy is like this:
1st meter: (1*30 µm) + 10µm = 40 µm
2nd meter: (2*30 µm) + 10µm = 70µm
3rd meter: (3*30 µm) + 10µm = 100µm
...
See also the picture:
Keywords: stl70, etl70, accuracy, magnetic tape, overall accuracy, hiperface, hiperface dsl, motion and drives, linear, motor feedback