web
You’re offline. This is a read only version of the page.
close
Support Portal

Avoid mutual interference of Dx50

Installation in order to avoid mutual interference.
Related Products
Dx50

Table of Contents

Murtal interference of DT50 - DT50HI - DL50

Minimum distance that must be maintained for parallel installation in order to avoid mutual interference between the sensors:

Murtal interference of DS50 - DL50HI

The DS50 and DL50Hi do not interfere with each other (mutual blinding can occur) so the values mentioned above are not relevant for the DS50 and DL50Hi. These sensors behave quite similar to Dx35 / DT50-2:

  • Installations with sensor alignments in opposite wise may be affected for low axial distance or for low angle between optical axes. Unlike Dx35/DT50-2, values for these limits are not available.
  • Installations in the same direction are not affected unless all the laser light is redirected (direct reflection) into the optical receiving area of the other sensor.
Keywords:
mutual interference, dx50