web
You’re offline. This is a read only version of the page.
close
Support Portal

[ICR8xx-4] Use the Conveyor View for investigations

Use the Conveyor View for the first simple investigations on the ICR to troubleshoot malfunctions.

Table of Contents

ICR890-4 Conveyor View Introduction

 

The conveyor view can be used in two different modes.

  1. Reading Gate Mode, conveyor is not in motion
  2. Aquisition Mode, with running conveyor
 

1. Reading Gate Mode

 

In default just the reading gate button is active which means all the parameters from reading gate sopas page will be displayed and can be helpful during the measurement of the system. In this mode a running conveyor will not be displayed.

  • It is possible to verify if the values for positions and angles are correct
  • The user can see if the default focus is as expected
  • The user can see if the release release points are behind the field of view
  • The reading area can be checked easy
  • The field of view can be verified 

 

The view itself look like follow and can be rotated by a left click or moved by an right click. Further there are some predefined views above ( Home, Top, Front, Left, Back)

 

 

2. Aquisition Mode

 

Conveyor View on a running conveyor

  • Option to see if the camera gets speed from controller
  • Option to see if the camera receive trigger data
  • Option to see slice data and polygon from VMS
  • Option to see if any barcode or vision label is read
  • Option to see the index and if it is assigned or not on stand alone devices
  • Capture log and replay 

To see the live data on a running sorter it´s requried to activate the "Acquisition Control" button

 

Not successful with your investigations? Please create a ticket with following information

Keywords:
ICR, ICR8xx, Troubleshooting, ICR890-4