web
You’re offline. This is a read only version of the page.
close
Support Portal

[IPCam] Save Image failed with Axis IPCam and SIM2000-p

IPCam was reachable but image could not be stored.
Related Products
SIM2000ST (1. generation, PowerPC)
SIM2000ST-C (3. generation, ARM)
SIM2000 (2. generation, ARM)
track and trace systems

Table of Contents

Save Image failed with Axis IPCam and SIM2000-p

The IPCam is receiving the trigger but the images cannot be stored on the PC

Indicator for this issue:

  • Successful Image Request from IPCam is counting up
  • Save image failed is also counting up!

 

1. Validate if the credatials of the IPCam are correct

 

2. Validate if an firewall is active. If yes check if the image transfer is working without the firewall. If this is the case, set up the specific firewall rules 

 

3. Validate if the image transfer is working on your PC by using image FTP

 

 

Not successful with your investigations? Please create a ticket with following information

Keywords:
IPCam, Axis, SIM2000-p