What is the maximum adjustment angle of the BEF-AH-DX50?
What is the maximum adjustment angle of the BEF-AH-DX50?
Related Products
BEF-AH-DX50 ADJUSTMENT BRACKET
Dx50-2
Dx50
Dx35
Table of Contents
The maximum adjustment angle is not exactly specified. This bracket is more for fine adjustment of the sensor. As a guideline, the maximum angle in the horizontal direction to the center line is about ±5° and in the vertical direction it is about ±3°.
+-
Keywords:
fine adjustable bracket
fine adjustable bracket