Support Portal

Inspector83x firmware releases

Firmware for Inspector83x.
Related Products
Inspector83x

Table of Contents

Firmware file and installation

The Inspector83x firmware file is linked to through the Download button at the bottom of this article. The zip file consists of firmware file (.spk), API documentation and release notes.

Installation

Use the SICK AppManager software to update the firmware in a device.
In the SICK AppManager, do the following to update the firmware:

  1. Connect to the device.
  2. Clear apps and user data on the device before upgrading to ensure disk space availability (recommended)
  3. Import the firmware package (*.spk file) to the right pane named “Firmware” using the “Add Packages to repository”/+ button or drag-and-drop.
  4. Select the firmware package, then press “Install” to start the firmware update.

Inspector 83x firmware release V3.8.2

- Fixed Edgematcher (Object locator) scaling causing wierd matches and low score

- Fixed digital output stop working if illumination type changed without first deactivating the output

Inspector 83x firmware release V3.7.0

Keywords:
firmware, inspector83x, firmware release, inspector83x firmware, inspector83x firmware release