web
You’re offline. This is a read only version of the page.
close
Support Portal

Mixing WLL80 and WLL180T in a gang mount setup

Related Products
WI180C-PB FIELD BUS GATEWAY
WI180C-PBS01 FIELD BUS GATEWAY
WI180C-B404 LOGIC MODULE
WI180C-PN PROFINET GATEWAY
WI180C-EC ETHERCAT GATEWAY
WI180C-EN ETHERNET/IP GATEWAY
WI180C-PNS01 PROFINET GATEWAY
WI180C-IOA00 IO-LINK GATEWAY
WI180C-IOB01 IO-LINK-GATEWAY
WLL80
WLL180

Table of Contents

Using different amplifiers like WLL80, WLL180T and AOD1 in a gang mount setup is possible.
However, there are some restrictions to consider for e.g. the correct sensor order.

 

As an example you can see below the WLL80 fiber amplifier in combination with other sensors that support this feature.
(Extract from the operating instructions of WLL80)

 

 

Limitations

In general WLL80 fiber amplifier and WLL180T fiber amplifier base- and expansion-units can be mixed when they are used in a gang mount setup. Detection will work for each sensor (power supply via bus-connector works in such mixed setup).

Functions (like "parameter copy" / "all-teach-in" / "anti-interference" etc.) that require internal bus communication will not work!
These features are only available when not mixing different device types (like WLL80 and WLL180T).

 

Keywords:
wll80, wll180t, bus, gangmount