web
You’re offline. This is a read only version of the page.
close
Support Portal

Analytics PC Cleanup Procedure

Steps to clean up Analytics PC
Related Products
Baggage Analytics
Logistics Diagnostic Analytics
Package Analytics
Tire Analytics

Table of Contents

PC Cleanup Steps

Windows

1.)  Go to "Programs and Features" or "Installed App" depending on the version of Windows.

2.)  Look for Analytics and Analytics Patches.  Always uninstall the Analytics Patches from newest to oldest.  Then uninstall Analytics.  In the event of a failed uninstall continue with the rest of the steps and then refresh "Programs and Features" or "Installed Apps" to clear the entries.

 

3.)  In "Programs and Features" or "Installed App" verify MySQL Server and MySQL Community are not installed.  If so, uninstall Server first

4.)  Open the Services panel and make sure there are no SICK or MySQL services listed.  As of Version 4.6.2, the services associated with the Analytics software are listed as follows:

  • SICK ActiveMQ Artemis (artemis-service)
  • SICK An AAP (lda-aap)
  • SICK An DACQ (lda-dacq)
  • SICK An Dynamic Dashboard (lda-dd)
  • SICK An Media Server (sick-bip-is)
  • SICK An MySQL (mysqllda)
  • SICK An Services (lda-services)
  • SICK Influx Service (influx-service)
  • SICK Node-red (sick-nodered)
  • SICK Support and Maintenance Service (ssms-service)
  • SICK Telegraf Service(sick-telegraf).
  • Older versions will list less services. 

 

If the services exist, follow these steps to remove them.  :

  1. Open the "cmd" as Administrator (or as SICK Privilege Elevation)
  2. Type the command "sc delete SERVICE NAME" at the command prompt.  The SERVICE NAME is found in the service properties. Access it by right clicking the service and selecting properties.  See the images below.
  3. Refresh the service list.
  4. The status of the service could be "disabled", but the service still may exist. Please, restart the machine in this case. Verify the MySQL service does not exist after the restart. 

5.)  Delete the folder MySQL from the "C:\Program Files", "C:\ProgramData", and "C:\Windows\Temp" if they exist.  Check other drive(s) if a different installation path was used.

6.) Delete all tomcat directories in "C:\Windows\Temp" if they exist.

7.)  If exists, C:\Program Files\SICK\Analytics Solutions folder and C:\Program Files\SICK\SickSupportAndMaintenanceService.  Check other drive(s) if a different installation path was used.

8.)  Delete the hidden folder "C:\Program Files\Zero G Registry".  If hidden files and folders are not showing, follow these steps:

      1. Click on File Explorer Options
      2. Click on View tab and under Advanced Settings and in the "Advanced settings:" locate "Hidden files and folders"
      3. Select "Show hidden files, folders, and drives"
      4. Click Apply and OK

9.)  Delete files from the folder "C:\Users\<User Login>\AppData\Roaming\MySQL" if any. Don't delete the folder "MySQL Workbench".

10:)  Go to C:\Users\<login username> folder and delete the "InstallAnywhere", ".InstallAnywhere", "_SICK Analytics Solutions_installation" and "_SICK Analytics Solutions [Version Number] Patch_Installation" folders

The typical user login for a Sick provided APU/PC is Engineering.  However, check all the other user login folders.  In the example below, the Systemadmin login was used to install an older version of Analytics and needs to be deleted.

11.)  In the Windows registry check for the existence and delete the following registry keys.

  1. HKEY_CURRENT_USER\Software\MySQL AB 
  2. HKEY_LOCAL_MACHINE\SOFTWARE\MySQL AB 

12.)  If it exists, delete the installer.properties file where the Analytics installation file(s) are located and ran.  If the installer.properties is left it can interfere with the Analytics installation and cause unintended results.

Keywords:
Analytics, Package Analytics, Baggage Analytics, Tire Analytics, Logistics Diagnostics Analytics, PA, BA, TA, LDA, Logistics, Logistics Analytics, Media Server, MS, clean up