web
You’re offline. This is a read only version of the page.
close
Support Portal

Dx35 What is the maximum tightening torque?

Related Products
Dx35

Table of Contents

Mount the distance sensor using the fixing holes provided. Note the permissible tightening torques of the screws:

  • When using the mounting accessories or equivalent construction: max. 1.2 Nm.
  • When using screws with a polyamide spot coating (according to ISO 8992): max. 2.0 Nm.
  • For any other type of connection between the device and screws: max. 1.0 Nm.
  • The connection between a screw and the housing of the device must be made using a washer (ISO 7092, for size M4) or an equivalent washer
Keywords:
mounting, tightening torque, dx35