Support Portal

The CCK KIT incremental encoder series

Additional information to the CCK KIT incremental encoder series - CCK25-CDA0-K01 - CCK35-CDA0-K01 - CCK40-CDA0-K01 - CCK45-CDA0-K01 - CCK50-CDA0-K01 - CCK53-CDA0-K01
Related Products
motor feedback systems
CCK
Attachments
TI_CCK-25-53-CDA0-K01_EN_910980103089_0805.pdf

Table of Contents

The CCK series was a motor feedback series for large hollow shaft motors. It was a completely open system. The customer had to mount the glass code disc on the shaft. The encoder electronic had to be mounted on the motors flange.

See also the data sheet in the attachment.

The CCK was an incremental encoder series. It had a sin/sos signal with 1024 periods per rotation and one signal with 1 sin/cos period per rotation. With this 2 signals, it was possible to do an absolute positioning within 1 turn.

It is more or less the incremental version of the SCK/SCL 25/53.

This Encoder series is phased out and we do not have any replacement.

Keywords:
cck25, cck35, cck40, cck45, cck50, cck53, motor feedback, encoder, incremental, kit, kit encoder