web
You’re offline. This is a read only version of the page.
close
Support Portal

Hiperface DSL Application Note 21, Safety requirements SAFEDSL008

Related Products
EES/EEM37
EFS/EFM50
EKS/EKM36
motor feedback systems
EDS/EDM35
Attachments
SICK-AN21-SAFEDSL008_Details-E269005_02a.pdf

Table of Contents

What is the content of the application note?

The HIPERFACE DSL technology offers the possibility for standard as well as safety related applications. For safety related applications there are additional measures defined to watch the system and to ensure its correct function or identify deviations to be able to bring it to a safe state. Therefore some SAFEDSL*** requirements are listed within the safety chapter of the manual which need to be fulfilled.

 

Within the Application Note 21 (Safety requirements SAFEDSL008) SICK provides information and general recommenddations how to fulfill the SAFEDSL008-requirement including information about different available channel resolutions and ways how get the information of an actual used motor feedback system.

The full application note is attached

Keywords:
Safety requirements SAFEDSL008, Safety requirements, Safety, SAFEDSL008, hiperface dsl, application note, motor feedback