Where is the position of the optical axis of a sensor mounted inside TPCC cooling housing?
Related Products
Table of Contents
In the download area of the TPCC cooling housings there are 3D CAD files (e.g. *.STEP) which showing the cooling housing together with the respective sensor as a simplified unit. The position of the sensor corresponds to the real position after screwing the sensor to the cooling housing. Together with the design drawings and dimensional drawings in the operating instructions of the sensor, the position of the optical axes can be determined.
Example for TPCC with sensor DT1000/DL1000:
- Section from CAD model:
- Section from design drawing in operating instruction
3. Section from dimensional drawing in operating instruction:
tpcc, optical axis, position, cooling housing, align, peltier, sensor