web
You’re offline. This is a read only version of the page.
close
Support Portal

SIG200 Logic-Editor: SLT (smart-light-tower) indication for different distance values

Related Products
SIG200-0A0412200 SENSOR INTEGR.GATE
SIG200-0A0512200 SENSOR INTEGR.GATE
SIG200-0A0G12200 SENSOR INTEGR.GATE
Dx50-2
SLT060-0B010J700 SMART LIGHT TOWER
Dx35

Table of Contents

In general, there are two possibilities to realize a distance/status display with the SLT and the SIG200.

Possibility 1: SLT "fills up" depending on the distance

The following points are to be done:
  1. Setup SLT:
    1. Process data to "Level Meter Mode"
    2. Adjust lights: Colors and Style (continuos or flashing) of the segments
  2. Setup SIG200:
    1. Upload IODD and assign to the correct ports
    2. Connect devices
       
  3. Edit Logic editor -> we need to convert the distance for "Level Meter Mode" into values between 0 and 100.

Possibility 2: SLT as a status indication

Application example: We want to display 4 different areas:

  1. green: dist > 2000 mm
  2. yellow: 2000 mm > dist > 1000 mm
  3. red flashing: 1000 mm > dist > 10 mm
  4. red: dist < 10 mm

We can use the "alarm indication" with the SLT. For this, profiles for 3 alarms can be selected (colors can be defined flexibly for each profile). We can then specify which profile is to be displayed with a 1, 2 or 3 on the variable.
For the 4th section, we can use the "Signal lamp mode" of the SLT and make all the tier's flashing red.

 

The following points are to be done:

  1. Setup SLT:
    1. Process data to "Signal lamp mode"
    2. Adjust lights: Colors and Style (continuous or flashing) of the segments and define the alarm profiles
  2. Setup SIG200:
    1. Upload IODD and assign to the correct ports
    2. Connect devices
       
  3. Edit Logic editor -> we need to switch the alarm indication depending of the distance to 1, 2 or 3. Also we have to set Tier 1-5 on if the distance is in a specific range.
Keywords:
level meter mode, signal lamp mode, alarm indication, logic editor