web
You’re offline. This is a read only version of the page.
close
Support Portal

no height measurement possible with RAY26

The Ray26 sensors are not suitable for height measurement.
Related Products
RAY26 Reflex Array

Table of Contents

The Ray26 sensors are not suitable for height measurement.
There is no measurement value available showing the degree of reflector covering.
The IO-Link Process Data supports only QL1 & QL2, Bit2-15 are not used!
 
The index 180 "Current receiver level (live)" only displays the receive signal of the weakest receive channel! Sensor has 5 internal channels and if another channel gets weaker the value of this channel is showed.
Keywords:
height measurement