web
You’re offline. This is a read only version of the page.
close
Support Portal

How do I mount the LPC-DX50 and Control Panel Cover on the Dx50?

Related Products
LPC-DX50 LENS PROTECTION COVER
CONTRO PANEL COVER W. PANE
Dx50

Table of Contents

The LPC-DX50 (2049269) can be used to protect the front screen of the sensor from damage caused for example by flying sparks and welding beads.


Align the cover in front of the front screen of the Dx50 sensor and use the snap hook on the cover to attach it to the sensor. Check that the cover is firmly in place.
In addition, it is possible to use a control panel cover (2058007) when using the front screen protection (the control panel cover cannot be attached separately without the front screen protection). For this purpose, there is a small recess in the front screen protection for attaching the control panel cover. 

Keywords:
protection, control panel cover, LPC-Dx50, Dx50