Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
If you are having trouble logging in or would like to register a new user, click below to get assistance.
How to setup the GLS100L for mixed operation with Lane Guidance and Code Detection
Example for GLS100L-1MEB1FZ with CANOpen.
The Configuration is done via IO-Link and SOPAS ET. A SiLink2 IO-Link Master may be necessary.
1) Operating Mode
select “Lane Guidance”
2) Code Reading
we use Multi Code or Code Tape (default)
Note: QR-Codes are not supported in Lane Guidance Mode, but DataMatrix Codes.
The example was created with SOPAS ET, for this the SiLink2 master is required.
There are a few rules for CANOpen that should be followed when configuring the process data:
Please note: All settings shown below can also be made with the CANOpen automation system - in most cases.
For this purpose, we provide a device description file, which can be downloaded from the website.
This file is called "EDS-file" = Electronic Data Sheet.
1) TPDO 1
X-Y- Position - only needed for Multi Code usage.
It is not relevant for Lane Guidance Mode.
2) TPDO 2
Data usable only for Code Navigation Mode.
3) TPDO 3
Tag ID, X-Y-velocity
4) TPDO 4
Lane Status, Guidance Data for up to 3 Lanes
5) TPDO 5
Lane Angle, Y-Position
6) TPDO 6
Tag-ID code tape, X-position
7) TPDO 7
X-position of the Third Code Tape
Example for Lane Guidance Mode with changed TPDO Mapping
To keep the number of TPDOs low, the data content can be mapped individually.
In the following example, the required data is reduced to three TPDOs.
1) TPDO 13 x Color Tape guiding position + Lane Status / Quality
3 x Color Tape Angle + Distance
Tag-ID MultiCode & Position of the code tape center