Support Portal

What does linearity and repeatability mean?

What does linearity and repeatability mean for the Magnet Angle Sensor MAS?
Related Products
MAS

Table of Contents

In the datasheet of our Magnet Angle Sensor MASQ47-36PEKU1SA10 Part no.: 1113979
is written:
 


 

What does that mean?

Linearity error

Is the range of the deviation to the correct value
example: real value is 180° ==> sensor value can be in the range from 179° to 181°

Repeatability

Is the range of deviation when you move to the same position once again
example: measured value is 180°. After another turn the measured value can be in the range from 179.7° to 180.3°.

Keywords:
MASQ47, linearity, repeatability