Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
The Inspector85x firmware file is available in the zip file linked through the Download button at the bottom of this article. The zip file consists of firmware file (.spk), API documentation and release notes.
Installation
Use the SICK AppManager software to update the firmware in a device. In the SICK AppManager, do the following to update the firmware:
Connect to the device.
Clear apps and user data on the device before upgrading to ensure disk space availability (recommended)
Import the firmware package (*.spk file) to the right pane named “Firmware” using the “Add Packages to repository”/+ button or drag-and-drop.
Select the firmware package, then press “Install” to start the firmware update.
- Fixed digital output stop working if illumination type changed without first deactivating the output.
- AI Object Detection (dStudio) in Nova 2.10 is supported in this version (please note that on-device AI Object Detection is not supported - please use 3.11.1 or later).