web
You’re offline. This is a read only version of the page.
close
Support Portal

SRM50-HZA0-S28 (1050103); SRS50-HZA0-S28 (1050102) special encoder

Table of Contents

The ...

  • SRM50-HZA0-S28 (1050103)
  • SRS50-HZA0-S28 (1050102)

... are special encoders with the following attributes:

  • 1024 SIN/COS periods per revolution
  • Absolute position with 15 bit per revolution (32'768 steps)
  • Customized stator coupling
  • plug in shaft
  • metal rubber stator coupling
  • It is free to order, or please contact the motor supplier

The SRM50-HZA0-S28 (1050103) is the replacement for the SRM50-HZA0-S08 (1034148).
The SRS50-HZA0-S28 (1050102) is the replacement for the SRS50-HZA0-S08 (1034208).

 

see also the drawing and the attached data sheets (unfortunately, the data sheets are only in German available)

Keywords:
srs50, srm50, hiperface, special, customized, encoder, motor feedback