web
You’re offline. This is a read only version of the page.
close
Support Portal

Are all programmable DFS2x encoders programmable?

Related Products
DFS2x
incremental encoders

Table of Contents

Programmable DFS2x encoders are recognizable at the electrical/communication interface "P".

Programmable is then the output type HTL or TTL as well as the pulses per revolution, the electrical/mechanical zero pulse width and the counting direction.

But this is NOT working with all programmable DFS2x encoders. The decisive factor is which connection type the encoder has.

In the picture below you can see the PIN assignments of all available connection types.

You also see what connection types are NOT programmable. DFS2x encoders with

  •  MS, 7-pin connector 
  •  MS, 6-pin connector 

 

WHY?

Due to the fact that the PGT's need both signals from the marker, so "Z" and "ZN" (or Z/), for the programming process, those connection types just have the signal "Z".

Therefore, the "programmable" DFS2x encoders with a MS, 7-pin or MS, 6-pin connector are not programmable.

Keywords:
programmable, DFS2x, incremental, encoders, connection type, MS 7 pin connector, MS 6 pin conector