web
You’re offline. This is a read only version of the page.
close
Support Portal

LMS4000 laser spot behaviour

In the operating instructions we state the following:- typically 4 x 3 mm (viewing window)- 2.5 x 2mm (3m distance)
Related Products
LMS4000

Table of Contents

In the operating instructions we state the following:
- typically 4 x 3 mm (viewing window)
- 2.5 x 2mm (3m distance)




x - axis: distance
y - axis: laser spot diameter


Dotted blue line: Due to the focusing, the spot initially decreases (in contrast to many other SICK LiDAR sensors) after exiting the device. The focus point is approximately 6m in the scanning direction. After that, the spot gets bigger again.
Keywords:
laser, spot, divergence