Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
What happens when the internal memory of the sensingCam SEC100 is full or the max. number of elements has been reached?
Article No: KA-09986
Version: 1.2
Subject to change without notice
Related Products
SEC100-5C9D1SFZZZZ SENSINGCAM
SEC110-5C9D1SFZZZZ SENSINGCAM
sensingCam SEC100
Table of Contents
When the internal memory (~6 GB) is full and further events or snapshots are triggered, the oldest files are automatically deleted.
If the file size of the snapshots or events is so small (low resolution, high compression...) that the maximum number of 1024 files in the archive is exceeded, the oldest files are also automatically deleted.
When a running event recording reaches the memory limit, it is stopped and saved. Afterwards, if another snapshot or event is triggered, the oldest file is deleted again - see above.
Alternatively, the FTP/SFTP function can also be used to send files directly to the corresponding server without using the internal memory.