web
You’re offline. This is a read only version of the page.
close
Support Portal

Measurement Errors LMSxxx

Related Products
LMS1xx
LMS5xx

Table of Contents

What is the statistical error ?

A statistical error means, when you do several measurements, you won't get the same value every time. Also when you take a measuring tape and do the same measurement several times, you will not get the exact same value every time.

 

What is the systematic error ?

A systematic error depends on the measurement principle and on the construction variation of the scanner.

 

What is the maximum error ?

The maximum measurement error of a device is the sum of the statistic and the systematic error. You can get such an error only when you just look at one measurement value, because, as more scans you take, the statistic error gets smaller because you can take the mean value of all scans.

 

Values for LMS1xx and LMS5xx

LMS1xx
  Typical Maximum
Systematic error ± 30mm ± 40mm
Statistical error 12 mm 20 mm

 

LMS5xx
  Typical
Systematic error  
SR 1..10m ± 25mm
SR 10..20m ± 35mm
SR 20..30m ± 50mm
HR 1..10m ± 25mm
HR10..20m ± 35mm
   
   
Statistical error  
SR 1..10m ± 6mm
SR 10..20m ± 8mm
SR 20..30m ± 14mm
HR 1..10m ± 7mm
HR10..20m ± 9mm

Unregular objects


When the object surface is not flat but irregular and especially, if within one single laser spot, there is some distance change to LMS5xx, will the output of the detected distance value to be the average distance or the nearest distance, or other situation?
We cannot give an defined answer to that question, but here are some notes that may help:
* generally the distance value depends on the energy that was reflected from the object. the generation of a real measurement value depends on weather there was enough energy reflected. For example if the nearer part of the object is reflecting a lot of light, that you may measure a short distance, compared to an object that reflects the same energy over all it's surface.
* We had a look at the special case, what is happening if the target is skewed. Some time ago there have been measurement, where the target was skewed in steps of 10°. That had nearly no influence to the distance value, so the result was, the measured value was over all distances not far away from the mean value. So we can say it depends always on the target and it's remission. If you take a real bright target, results can be different.

Keywords:
Errors, Issues, Known problems, Measurement errors, Statistical error, Systematic error