Support Portal

AN: Integration of RFH5xx in Beckhoff PLC with SIG350 via EtherCAT

Tutorial how to integrate a RFH5xx with a SIG350 to a Beckhoff PLC via EtherCAT.
Related Products
RFH505-1004301 RADIO FREQUEN. SENSOR
RFH510-1004301 RADIO FREQUEN. SENSOR
RFH515-1004301 RADIO FREQUEN. SENSOR
SIG350-0006AP100 IOL-MASTER,ECAT
RFH5xx
SIG350 EtherCAT
Attachments
Connect-RFH5xx-to-Beckhoff-PLC-with-SIG350-V1_1.pdf

Table of Contents

Introduction

The application note provides instructions for integrating the RFH5xx into a Beckhoff PLC using the SIG350 as an IO-Link master. The application note also contains examples for reading the UII and reading service data (ISDU parameters).

Application Note is attached as PFD file for download.

Keywords:
rfh5xx, Beckhoff, PLC, RFH505, RFH510, RFH515, SIG350, EtherCAT