Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Stream Setup release. Software used for connecting to and configuring Ranger3 and Ruler3xxx devices.
Related Products
Ranger3
Ruler3000
Table of Contents
Below you can find the latest release of Stream Setup. The download requires you to authenticate via SICK-ID. If you require a version not present here, please contact your local SSU for assistance or generate a support request.
Stream Setup 10.1.0
This release contains the following improvements:
Support for more than 2 cameras when using the alignment tools.
Single target alignment with 1 to N cameras.
Alignment can now be done on cameras with reversed motion direction.
Alignment tools now support Ranger3 cameras in addition to Ruler3000 cameras.
Encoder resolution calculation wizard to help with encoder setup.
Usability improvements when working with speed, profile rate, Y resolution, etc.
This release has a new tab for aligning Ruler3000 cameras mounted side-by-side to get a stitched image. Firmware version 4.2 is needed for this feature. This release also has support for loading mv3 files. See release notes for further details.