web
You’re offline. This is a read only version of the page.
close
Support Portal

What is the diameter of the light spot for Dx50 / Dx50-2?

Related Products
Dx50-2
Dx50

Table of Contents

The light spot diameter of the Dx50 and Dx50-2 depends on the distance and temperature. The diameter can be calculated as follows - the calculator setting must be DEG:

at +20 °Cdiameter [mm] = 4 mm + 2 * tan(0.025) * distance [mm]

Typical light spot dimension:

  • 20 m -> approx. 21 mm
  • 30 m -> approx. 30 mm
  • 50 m -> approx. 47 mm


Please note: The actual light spot diameter can vary from one sensor to another by up to +/- 20%.

Keywords:
light spot diameter, dx50, dx50-2