web
You’re offline. This is a read only version of the page.
close
Support Portal

Troubleshooting: RFH5xx EtherNET/IP functionblock

This document provides assistance with problems when using an EtherNET/IP function block of the RFH5xx with use of the SIG200 EtherNET/IP.
Related Products
RFH505-1004301 RADIO FREQUEN. SENSOR
RFH510-1004301 RADIO FREQUEN. SENSOR
RFH515-1004301 RADIO FREQUEN. SENSOR
RFH5xx
SIG200 EtherNet/IP

Table of Contents

Possible problems with RFH5xx EtherNET/IP FB:

When using the RFH5xx in combination with the SIG200 EtherNET/IP, problems may occur which are indicated in the function block. 

 

Possible error pattern:

  • FB returns timeout error
  • Other unexpected error codes are returned by the FB
  • Data from SIG200 does not arrive at the PLC

This may be due to incorrect parameterization of the timing.

Solution

In most cases, timing problems are caused by incorrect parameterization of the RPI (Requested packet interval). If a SIG200 is used, the default RPI time must be set <= 10ms to ensure stable data transmission. 

 

If this solution does not solve the problem, please create a support ticket.

Keywords:
troubleshooting, RFH5xx, RFH505, RFH510, RFH515, Ethernetip, EtherNET/IP, troubleshooting rfh5xx, SIG200, Functionblock, Mitsubishi, OMRON