Support Portal

Download REST API device description file from sensingCam SEC100

Related Products
SEC100-5C9D1SFZZZZ SENSINGCAM
SEC110-5C9D1SFZZZZ SENSINGCAM
sensingCam SEC100

Table of Contents

Since firmware version 1.2.0 of the sensingCam SEC100, the device description file can be downloaded directly from the camera itself. The following endpoint is to download the file:

           

[IP-Address]/deviceDescription.yaml

The file is in YAML format. A connected sensingCam SEC100 is required to download the file.

Note that the device description does not include code for authentication.

Keywords:
device description, openAPI, RESTAPI, REST, YAML