web
You’re offline. This is a read only version of the page.
close
Support Portal

"locating lug" or embossing detection on turning bottle with fiber

"locating lug" or embossing detection on turning bottle with fiber
Related Products
LL3-DT01S01 OPTO FIBRE L=1500MM
LL3-DT01 LIGHT GUIDE
LL3-DT01-05 LIGHT GUIDE
LL3-DT01S02 LIGHT GUIDE
WLL80
WLL180

Table of Contents

Task:

Customer needs a solution for the "locating lug" detection that he can align the bottle before labelling.

Customer advised that the bottle will rotate on it's center and is extremely smooth.

our proposal:

Fiber-optic sensors eg. WLL80 and suitable proximity fiber like LL3-DT01 #5308076 mounted in an angle of 45degree to the bottle to detect the edge of the lug.

actual values of Fiber-optic sensors:

bottle surface during turning max 800digits

edge of the lug 9999 digits

important points:

alignment of the bottle = fiber head to bottle distance has to be stable,

if the lug or embossing is small or you need more flexibility with the light spot diameter/ distance to the bottle you can use a prox fiber LL3-DM02 #5308071 with screwable/ adjustable lens LL3-DA06 #5326468

pictures:

Keywords:
bottledetection, notch, packaging, turning bottle