web
You’re offline. This is a read only version of the page.
close
Support Portal

How to configure the process data for the GLS100L with CanOpen interface

Important configuration options for process data related to the CANopen version of the GLS100L.
Related Products
GLS100

Table of Contents

CanOpen Settings, available in SOPAS

For the GLS100L with CanOpen interface, it is possible to configure the process data via SOPAS ET.
A SiLink2 IO-Link master is required for this, which can be ordered as an accessory part.

Automatic Start

What does “Automatic Start“ mean?

 

After power-up, the device enters operating mode immediately, and transmission of the Transmit PDOs begins right away (depending on the PDO configuration).

 

For the GLS100L, the default setting is “AutoStart”.

 

Otherwise, data transmission must be initiated by the NMT master (NMT = Network Management).

Here are some sample screenshots created with PCAN-View:

Activation or Deactivation of the Transmit-PDOs

  • three PDOs are activated by default
  • up to 7 PDOs can be activated  in total for the GLS100L
  • a maximum of 8 bytes of data content is available for each PDO
  • for each activated PDO, a "COB ID" must be assigned, the COB ID also contains the node address
  • however, only up to 4 COB IDs can be assigned under the same node address

Attention:

if more than 4 PDOs are needed, the surplus ones must be accommodated under a still free node address.

Determination of the "Transmission Type"

The default setting for the transmission type is 255 = event-driven

 

This means:
The PDO is triggered either “on change” or via the event timer.

 

For the GLS100L, this means:

A “change” occurs every time the image is updated, which typically happens about every 33 ms.

 

Attention:

if the set time for the event timer is longer than the shutter time of the GLS100L, then the cycle time is based on the image capture time

PDO Mapping

The content of each PDO can be configured individually, considering the maximum data length of 8 Byte.

 

Attention:

There is no monitoring of the maximum data length in SOPAS.

Keywords:
automatic start, PDO, TPDO, Mapping, CanOpen, NMT, Node Address