Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
How to connect external illumination to Inspector83x
Article No: KA-10579
Version: 3.0
Subject to change without notice
Related Products
InspectorP63x
InspectorP61x
InspectorP64x/InspectorP65x
InspectorP62x
Table of Contents
This article explains how to connect external illumination to an Inspector83x. The external illumination can be connected directly to the camera, or via a CDB650 or CDB620/CDM420.
Two types of external illumination are covered in the article:
ICL – external illumination with trigger input The ICL has an M8 connector with 3 pins (supply voltage, GND and trigger input).
VLR – external illumination without trigger input The VLR has a M12 connector with only 2 pins (supply voltage and GND). It is possible to trigger a VLR directly from a CDB650, or with a Lighting trigger unit (SICK Part No. 2056990).
Please find more information on the Operating Instructions of the device.
Connect external illumination to external illumination connector
The Inspector83x has an external illumination connector (X2 in image below) from where VLR and ICL illumination can be powered, and ICL can be triggered.
The Nova versions (2.15 or later) supports connections with external light connectors. To trigger the external light from the camera, configure the Digital Output 7 or 8 to "External light".
The M8 to M12 Connector with the SICK P/N : 2095731 can be used to connect the Inspector with the VLR M12 connector. With this connector, it is only possible to power the VLR.
In order to trigger the VLR, you need to use the VLR trigger cable (SICK P/N : 2134622) along with the M8 to M12 connector . In this case the connection looks like Inspector(X2 connector) --- M8 to M12 Connector --VLR trigger cable -- VLR illumination
Connect ICL to CDB/CDM
ICL illumination can be powered and triggered directly from both CDB650 and CDB620/CDM420.
To connect an ICL to a CDB/CDM you need an open cable end with three wires: supply voltage, GND and trigger input.
Connect the trigger input for the illumination directly to the switching output Res 2 or Res 4 of the Inspector83x in the CDB.
Power the illumination either via a separate external voltage connected to the GND for the CDB, or via the supply voltage which is connected to the CDB.
Note: The Uɪɴ supply voltage connected internally to the trigger unit is protected by the fuse 2 A of the CDB650. The total current for all consumers (CDB650 internal, InspectorP6xx including switching output Res 2 and illumination) must not exceed 1.5 A.
Note: The Uɪɴ supply voltage connected internally to the trigger unit is protected by the fuse0.8 A of the CDB620. The total current for all consumers (CDB620 internal, InspectorP6xx including switching output Res 2 and illumination) must not exceed 0.8 A.
Connect VLR to CDB/CDM
VLR illumination can be powered and triggered directly from a CDB650. To trigger a VLR from a CDB620 or CDM420, you also need a Lighting trigger unit (SICK Order No. 2056990).
Connect VLR to CDB650
To connect a VLR to a CDB650 you need an open cable end with two wires: supply voltage and GND.
To trigger the illumination its supply voltage is switched on and off via the load interrupter switch of the trigger unit integrated in the CDB650. The switching output Res 2 or Res 4 of the InspectorP6xx forms the control input circuit for the trigger unit.
Note: The Uɪɴ supply voltage connected internally to the trigger unit is protected by the fuse 2 A of the CDB650. The total current for the Inspector83x, including switching output Res 2 and illumination, must not exceed 1.5 A.
Connect VLR to CDB620/CDM420
To connect a VLR to a CDB620/CDM420 you need an open cable end with two wires: supply voltage and GND. You also need a Lighting trigger unit to trigger the VLR. The lighting trigger unit has an open cable end with 3 wires: supply voltage (red), GND (black), trigger input (yellow).
The example below shows how to connect a VLR to a CDB620.
Mount the lighting trigger unit on the CDB620, as shown in the illustration below.
Connect the trigger input (yellow) directly to the switching output Res 2 of the Inspector83x in the CDB620.
Power the trigger unit with the red and black wires, either via a separate external voltage connected to the GND for the CDB620, or via the supply voltage, which is connected to the CDB620.
Connect the VLR to the lighting trigger module at GND and L+.
Note: The Uɪɴ supply voltage connected internally to the trigger unit is protected by the fuse 0.8 A of the CDB620. The total current for all consumers (CDB620 internal, Inspector83x including switching output Res 2 and illumination) must not exceed 0.8 A.