web
You’re offline. This is a read only version of the page.
close
Support Portal

2D LiDAR Mutual Interferences (HDDM+)

This page explains how 2D LiDARs overcome mutual interferences with HDDM+.
Related Products

Table of Contents

Measurment technology HDDM+

HDDM+ measurement technology is in general robust against mutual interferences from other sensors. In HDDM+, each measurement point consists of several superimposed individual pulses. Depending on the scan profile (angle resolution and frequence) up to 254 pulses are combined for one measurement point. To prevent interference, the pulse timing is not fixed but random. This reduces the risk of the LiDAR synchronizing with another LiDAR in an unwanted way.

In the following video, five picoScans were placed at the same measurement height. The measurement results show that the availability of the device and the measurement data is not affected by either indirect or direct interference. Only slight measurement deviations are visible (upper wall in the video):

Mounting position

To rule out even the slightest effects on the measurement accuracy, the products should be arranged in such a way that as few laser beams as possible are received from other products.

Angle

Distance 200 mm

Keywords:
Robustness, influence, blending, hddm, LiDAR, mutal influence