web
You’re offline. This is a read only version of the page.
close
Support Portal

Cloning Parameters via SDV file from one device to another

Related Products
TiM
LMS1xx
LMS5xx
LMS4xx

Table of Contents

Abstract

How to import a parameter file from one device to an other via Sopas

 

SOPAS 3.xx and higher

Export parameter file


On the Sopas main page, click on the small drop down on the right top side of the device square:


and in the opening dialogue on "Export..."
Than choose a folder to save the file to.

 

Import saved parameters into a device

on the device square, open the same dialogue as before


and click on "Import..."
Choose the saved parameter file  (.sopas file)
and the import starts automatically:

Finish.

 

SOPAS 2.xx

save parameter file


Device is in Sopas:


Export the Parameters from first device by clicking on "Project/Export device":

Choose "Sopas Device file" in the following Window:

and finally choose a path to save to:

 

loading parameters into the device


After that you have a .sdv file in the folder, which can be used to be imported to another sensor.
This is done via:
"Edit/Load device data to device"


choose the saved .sdv file:

If you are not already logged in, type in the user level and the password (find it in the operating manual)

Then the upload starts:

Whe it has finished, replace the existing device in Sopas by the new one (requested in the wizard) and then you will have finished the parameter import.

 

 

Keywords:
SOPAS, Parameter file, Cloning parameters