Counting bottles with different height
The article illustrates how to count all kinds of bottles with different sizes by using a MLG-2 Pro.
Related Products
MLG-2
Table of Contents
Task:
Counting all kind of bottles with different sizes
- Bottles are close together - body to body
- different designs & labels
- can be opaque or semi transparent
Recommended sensor:
MLG-2 Pro with up to 4 x Q outputs
- Sensing area = in-between the bottle neck
Suggestion for setup:
- configure different zones for each bottle height
- configure the output function - for each size one Q output
- watching the result
Benefit MLG versus WLXX(G) single beam system:
- no movement of sensor after changing bottle size - one sensor for all kind of bottles
- more reliable thanks to multi-beam system in case of critical transparent bottles
- Flexible change of configuration to reach best detection results
- up to 4 Q outputs can be used, so that each Q output corresponds to one bottle size
Keywords:
counting bottles, counting bottles with different height
counting bottles, counting bottles with different height