Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Field Analytics 1.3.3 is a security patch targeting potential vulnerabilities related to older versions of MySQL and Artemis service.
Bugfixes
FA 1.3.3 Patch – MQTT Datasource Fails Due to Connection Loss Observed in Logs FA 1.3.3 – InfluxDB data folder is incorrectly named as "Data" instead of "Influx Data" when installed on a non-default drive (e.g., E:/) FA 1.3.3 Patch Resolves "Failed to Start My SQL Service" When Database Is Installed on Non-Default Drive Exceeded Data Source Limit" Error Despite Valid License – FORD Site FA 1.3 + FA 1.3.3 Patch > After applying the Field Analytics (FA) 1.3.3 Patch on top of the FA 1.3 Release build, the Artemis service fails to start automatically. FA 1.3.3 Patch > After applying the latest patch upgrade, the OPC UA/ OPC DA data source health status changes to "Error", resulting in no data being stored in Historian. FA 1.3.3 > InfluxDB service fails to start when installed on a non-default drive (e.g., E:/). FA 1.3.3 Patch > MySQL Version Not Upgraded to 8.4.5 During Patch Installation FA 1.3.3 > OPC UA Data Source with "UsernamePassword" User Identity Type Fails to Connect – Displays '?' or Error Symbol FA 1.3 + FA 1.3.3 Patch > Accessing the About Info page results in a 412 Precondition Failed error, and build details are not displayed in the UI. FA 1.3 + FA 1.3.3 Patch > Clicking on Historian results in a 500 Internal Server Error from the backend. FA 1.3.3 > [OPC UA] Data Source Health Status freqently Flickers Between OK and Error States Intermittent > FA 1.3.3 > Users encounter a blank page when accessing the Data Source or Media Server. FA 1.3.3 > MS images are failing to load in the Historian and return a 404 Not Found error. Backend logs indicate that the Media Server encountered an issue when attempting to access the Media Server URL. Flexi Soft 8th bit shift causing desync between 8th bit in flexi soft data set and 8th bit in FA Update preferences column FA 1.3.2>Tabular> Duplicate FA 1.3.3> Tabular> BE is providing the records paginated incorrectly and grouping the DS name instead of event time Old Data Sources show "Error" Health Status despite active and online related Requests/Data. LINUX - Verify after installation LICENSE_ANALYTICS.txt is present in FA installation folder. Patch- Verify after installation LICENSE_ANALYTICS.txt is present in FA installation folder. Verify after installation LICENSE_ANALYTICS.txt is present in FA installation folder. FA 1.3.3> Unable to perform Historian Search , getting 500 Internal Server error. FA 1.3.3> MySQL version is not updated to 8.4.5 in Linux. Add license file part of patch and full installers FA 1.3.2> BE is providing the records paginated incorrectly and grouping the DS name instead of event time for Pivioting search Update FA 1.3.3 with Latest PubSub Bridge Version and Add License File Testing the latest Pub-sub bridge version. FA 1.3.2: Historian Dataset download limits issue. Intermittent > OPC UA > Editing OPC UA Data Source Triggers 500 Internal Server Error Upgrade FA with Mysql 8.4.5 FA 1.3.2:OPC UA issues. Node-red> User is shown with login page when navigation to node-red page inside the application
Customer required actions
Please upgrade to 1.3.3 as soon as possible. For users with 1.2.X or older, please use the patch installer to upgrade to 1.3.0 first before patching to 1.3.3.
Hardware & software compatibility
Operating Systems:
Windows 11 (64 bit)
Windows 10 (64 bit)
Windows Server 2019
Windows Server 2022
Linux Ubuntu 22.04
Linux Ubuntu 24.04
Required Disk Space
Depends on application. Contact SICK product support for hardware
requirements.
Minimum 2 GB for installation. 3-4 GB SSD Recommended
Required Disk Type
Solid State Drives (SSDs) with high-write endurance are highly recommended.
Processor
Minimum Intel Core i5
Recommended i7 (2.30 GHz)
Memory (RAM)
16 GB DDR3L or higher is recommended.
Screen Resolution
1920 x 1080 (16:9) aspect ratio is recommended for optimal viewing.
Browsers
Google Chrome (Version 140.0.7339.186)
Mozilla Firefox (Version 140.0.7)
Microsoft Edge (Version 140.0.3485.81)
Pre-requisite software
Java Runtime Environment 17.0.6
MySQL 8.4.5 (MySQL Database is recommended for sites where heavy
load is expected)
Influx v2.7.1 (Influx Database is recommended for historian to store the
records)
Runtimes and Databases are bundled with the installation package and will
be installed/updated automatically if they do not exist on the target machine
Known limitations & issues
Limitations
User Manual> Multiple spaces are being added between the words in most places.
User Manual> "Refer to _Ref123046425" is displayed in most of the places where images are being referred.
User Manual> When user refresh or navigate to some other feature then same page in User Manual is not retained.
User Manual> When user expands the User manual I-frame then it is not getting resized properly.
User Manual> When User Manual is opened in new tab then there's no space in between "FieldAnalyticsUserManual".
User Manual> When user clicks on three ellipses and again click on it then 'FieldAnalyticsUserManual' is displayed for microsecond.
User Manual> 'Close' help text is displayed for exiting the User manual window and for TOC.
User Manual> Numbering is incorrect in most of the places in the document.
User Manual>Misalignment of the texts/contents in various sections i.e., Introduction, Edit_Alerts sections, UserManual, ServerDateTime etc.
User Manual> Texts and the contents under the section is unstable and flickering.
User Manual> Search in user manual is broken when search with single/multiple words.
User Manual> When user click on home icon on the expanded user manual then it is getting navigated to random pages in the manual.
Node-red> User is shown with login page when navigation to node-red page inside the application.
Davinci bar chart widgets > User is not able to view complete data in the created widget when the X axis has more than 50 values.
FA 1.3.3 – InfluxDB data folder is incorrectly named as "Data" instead of "Influx Data" when installed on a non-default drive (e.g., E:/)
Intermittent > FA 1.3.3 > Users encounter a blank page when accessing the Data Source or Media Server.
For artemis and pub-sub services activating auto-restart the Artemis service is displayed for FA 1.3.2 full and patch.
Application is crashing on trying to create DS with huge json payload
Historian > MQTT DS > extra record is appearing when user create 2nd DS with same MQTT nodered flow.
DB user is not able to login
Incorrect validation message is shown even with valid selection of fields in historian
Pie Chart > Hover texts are truncated on pie chart when the data is appearing on top or bottom
Data retention is reverting to default values after FA 1.3 upgrade
Widgets> After clicking on Confirm then a pop-up snackbar message gets changed.
LDAP user group mapping > user have no ways to delete assigned groups when the LDAP user was deleted from Active directory server
Data Source> When user is cloning multiple DS then the focus is getting removed from that particular DS.
Dashboard Context> The 'Copy ID' option is displayed for the Untracked Images folder.
Widgets moves out of the dashboard page while moving and not responsive to mouse movements
Data Source> When user changes the locale as well as the date time format then the date and time is not displayed accordingly.
Notification> Add/Edit Delete Notification rule and alert Keys are not user centric or localized
Modbus TCP DS > POST api/v1/dd/configure/datasource? API throwing 400 when 'device tag scan rate' value exceeds '9,999,999,999'
CLONE - Norca dashboard>Norca Error Percentage over time widgets> When there is single point data for selected time unit the x axis values shows in milliseconds.
CLONE - Norca Dashboard> The tooltip content is not properly visible when user hover on top portion of the Bar having more percentage or over the last Bar.
notification alert, Application settings > date format in date columns are not appearing acc. to date format set in personal setting.
Historian Issues
LDAP > Sickadmin and the privileged LDAP user is not able to modify roles which have "create user" privilege.
sickadmin/sickservice is not able to modify the administrator's LDAP role when authentication is set to LDAP.
CLONE - Data Source health Status > 'Updated at' timestamp is appearing incorrect
Localization> The user can see English words even when the locale is set to other than English.
Intermittent> Application not loading properly when logged in after some time
The "Source" on Add Widget page is not localized for supported locales.
Add Widgets>2D Schematic Widget> Tooltip is getting truncated when the sensor position is set on top.
TableWidget>Global search is not happening for the decimal digits having 0 value in Aggregated Read Rate table
Safety Device> The Search box for Normally Open column is not highlighted properly.
GET Locale API > multiple "?" symbol appearing in 'localName' value while changing locale in persanal settings
CLONE - Group Assigned to the AD user is not updating properly in a particular scenario.
Widget> Traversing of widgets is improper when using tab key to navigate on Add widget dialog.
Flex Chart Widgets> Selected legends get reset on resizing the widget.
Download Logs> Incorrect records count is displayed for in the Search field of Date Modified.
POST /api/v1/user >Firstname & Lastname char limit validation is not provided
license page > 'Mac' is appearing instead of "MAC" in snack-bar message.
Modbus TCP> When the creates the DS with Store Difference (Signed) then health status fluctuates between warning and Ok status.
HTTP Server DS >POST /api/v1/dd/configure/datasource returning 500 when user remove "mqttTopic" object from the datasource DTO
Privilege> When the user has "Create Data Source, Read Data Source and View Data Source" privileges then user is getting 403 response code.
User is getting navigated to the last viewed dashboard instead of the "default dashboard" when the user login to the application
POST /api/v1/dd/configure/datasource throws 200 instead of 412 when a data source is created with historical deadband set up to more than 8 decimal.
Widgets> When user switch from Transform function to Map Data Sources then "quot;" is displayed in the pop-up message.
Clone Dashboards>Message Key is appearing instead of String on snackbar message when cloning the dashboard
Data Source> When the health status is displayed as warning then no value is displayed in the "Last Successful At".
LDAP User> Manage User > Invalid privilege are appearing for the LDAP user.
Installer> Manage User> "Last Logged In Time" is displayed for the operator user even when he has not logged in.
License> When the user reload or refresh the page then Whiltelabel error is displayed. Also, Internal server error with 500 response code is displayed.
Surface Pro 7 device> DS> Select Refreshing Frequency tool tip is overlapping with the value.
Surface Pro 7 device> DS & Widgets > When the user selects the value from the dropdown then that value is not highlighted.
Personal Settings >PUT "/api/v1/mypreferencesetting?locale=en_US" is giving 412 instead of 200
Ldap> POST api/v1/settings/ldap/verifytest allows to verify ldap level settings returns with response code 404
Authentication> LDAP> Save button is enabled irrespective of the settings entered for LDAP and verified.
Ldap>GET /api/v1/settings/ldap/providerstest allows to fetch Ldap Providers returns with response code 404
Ldap>POST api/v1/settings/ldaptest allows to creation ldap level settings returns with response code 404
POST api/v1/settings/ldaptest returns with response code 405 instead of 404
Ldap>GET api/v1/settings/ldap allows to lists Configured settings returns with response code 404
Historian UI > When the user types the date on Custom date field then 'Invalid entry' is displayed.
BE >The exported CSV file from Swagger API does not match with the exported CSV file from UI.
Legal Information
For Software, Software as a Service or Products containing Software, the following terms and conditions shall apply: (i) SICK’s General Terms and Conditions for the Supply of Software Products (“AVB Software SICK”, available at www.sick.com). And/or (ii) SICK’s General Terms and Conditions for Software as a Service (“AVB SaaS SICK”, available at www.sick.com).
This work is protected by copyright. Any rights derived from the copyright shall be reserved for SICK AG. Reproduction of this document or parts of this document is only permissible within the limits of the legal determination of Copyright Law. Any modification, abridgment or translation of this document is prohibited without the express written permission of SICK AG.
The trademarks stated in this document are the property of their respective owner.