Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
This device gives the possibility to orientate the M12 Connetion plugs to the backside. Instead like standard upwards. Only the systemplug is different! This give the oppertunity to safe the built in hight space in a application. Be aware, that all the asseccories are built for the standard system plug with the M12 connector on the top! Only the Standard bracket are able to mount with the weatherhood.
Also the only weatherhood which fits is the weather protection hood 2063050:
In combination it looks like this: CAD Drawing in the attachment area...
Restrictions:
During mounting you need to consider the bending radius of the cables, which is minimum 90 mm, given by the 12-Pin cables. You can see from the pictures below, that approx. 14 cm from the device to the mounting position have to taking into account. Also with the mounting Kit 1+2 you don´t reach this distance. So there have to be found a individual soultion for each application.