web
You’re offline. This is a read only version of the page.
close
Support Portal

Intelletto Keyboard Raw Mode with Lector6xx

How Lector6xx interact with an Intelletto HID converter to send Keyboard Raw Mode
Related Products
fixed mount barcode scanners
image-based code readers
RFID

Table of Contents

This article describe how to send USB HID keyboard strokes.

For the conversion process, the separate hardware "Intelletto Ethernet to Serial & HID Keyboard Converter" is used.

Follow the attached manual to set up the output format or script in the Lector. The chapter for the keyboard raw mode can be found at page 11.

 

Some example for Lector6xx:

Keyboard stoke

Characters to send in HEX format

Output format editor

Do not use STX ETX

Script

F8

FD 00 41 00 00 00 00 00

local F8 = string.char(0xFD, 0x00, 0x41, 0x00, 0x00, 0x00, 0x00, 0x00)

 

 

 

 

Very important: Do not send any STX or ETX framing! Otherwise the Intelletto will not accept the RAW Keyboard characters!

 

When using a script, the framing can be configured with:

local success = ComChannel.transmit(hEthernetAux, outputString, true)

While "true" transmit the data without framing.

 

 

 

 

Example for Modifier Byte: Left SHIFT and Left ALT is pressed at the  same time.

 

 

 

Keywords:
Intelletto Keyboard