Mount IQ10 close together
Related Products
Table of Contents
We would like to install two IQ10 close together in an application.
The problem with inductive sensors is that the oscillating frequencies of the sensors disturb each other. Therefore, it is crucial to keep the distance written in the installation note between them.
If this is not possible and you have to mount it closer together it is no problem: for this reason, we have special sensors with changed oscillating frequencies.
However, you should leave a gap so that the heat can escape and the sensors do not overheat.
Here are some standard IQ10 with the special version behind to prevent crosstalk / false trigger.
IQ10-03BPOKT0S --> IQ10-03BPOKT0SS01
IQ10-03BPSKT0S --> IQ10-03BPSKT0SS02
IQ10-03BPSKW2S --> IQ10-03BPSKW2SS03
IQ10-03BPSKWDS → IQ10-03BPSKWDSS15
IQ10-06NPSKT0S --> IQ10-06NPSKT0SS06
IQ10-06NPSKW2S --> IQ10-06NPSKW2SS05
IQ10-06NPSKWDS --> IQ10-06NPSKWDSS08
That means that you have to use one standard sensor and one special sensor (or alternately) to mount close to each other.
mount iq10 close together, inductive sensor, oscillating frequencies, special sensors