web
You’re offline. This is a read only version of the page.
close
Support Portal

What is the purpose of the MaxCol (maximum change of level) function?

Explains the purpose and function of the MaxCol (maximum change of level) function in the LFP guided wave radar level sensor.
Related Products

Table of Contents

The MaxCol (maximum change of level) function of the LFP guided wave radar level sensor suppresses short-duration, high-amplitude signals that occur above the actual product level. Such signals are typically caused by jets of liquid during cleaning processes or by medium splashing against the sensor probe. Without suppression, these transient signals may be incorrectly interpreted by the sensor as valid level echoes.


The MaxCol function filters out signals that would otherwise result in implausibly rapid changes in the measured level value, thereby improving measurement stability and reliability.

Note


If the jet of liquid onto the probe continues for a prolonged period, the sensor may eventually interpret the signal as an actual level signal, causing an incorrect level reading. Once the liquid jet disappears, the MaxCol function slightly delays the return to the correct level reading.


Keywords:
MaxCol, spray ball