FlexChain - Empty Box Application
Related Products
Table of Contents
- I want to share one application example with You
- In that example we want to configure the FlexChain Host in such a way, that the switching output indicates if the box is empty or not.
Used sensors:
- 4 x GTB6 are watching if the box is empty
sensor 1….4 - 2 x GL6 as trigger sensors, sensing the wall of box
sensor 5 & 6 – blanking the front & back edge of box
Zone Configuration
we start with the Zone Configuration:
As you see, the Zones are equal to the sensor channels.
- Zone 1 = Qint 1 = Sensor 1
- Zone 2 = Qint 2 = Sensor 2
- and so on
according to the above picture:
sensors 1...4 = OFF status, sensor 5...6 = ON
Logic Configuration
next step is the Logics editor
- Logic 1 = sensor 1 … 4 detect no object
- Logic 2 = trigger sensor 5 & 6 = window enable
- Logic 3 = result = Box empty
Pin Configuration
next step is to do the Pin assignment
- Pin 4 = switching ON when box is empty
- Pin 2 = switching OFF when box is present
Process Data Configuration
Last but not least we have a look at the Process Data.
That is only necessary if Bus interface is used, for instance IO-Link or RS 485
In that example we use one of the pre-defined PD configurations - - see profile.
application example, Flexchain host, configuration, switching output , box empty