Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Download REST API device description file from sensingCam SEC100
Article No: KA-09939
Version: 1.1
Subject to change without notice
Related Products
SEC100-5C9D1SFZZZZ SENSINGCAM
SEC110-5C9D1SFZZZZ SENSINGCAM
sensingCam SEC100
Table of Contents
Since firmware version 1.2.0 of the sensingCam SEC100, the device description file can be downloaded directly from the camera itself. The following endpoint is to download the file:
[IP-Address]/deviceDescription.yaml
The file is in YAML format. A connected sensingCam SEC100 is required to download the file.
Alternatively, the file can also be downloaded via the web UI (since FW2.0.2).
Note that the device description does not include code for authentication.