Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
How does the heating of the Dx500 distance sensors work?
Article No: KA-09321
Version: 1.0
Subject to change without notice
This article describes how the heating of the Dx500 distance sensors works and how the heating power can be increased if necessary.
Related Products
Dx500
Table of Contents
The heating variants of the Dx500 (Dx500-x2xx, -x4xx, -x6xx) contain a flat heating element. If the internal temperature of the unit falls below -10 °C, the heater is automatically activated; if it rises above 0 °C, it is deactivated again. These switching points are fixed and cannot be changed.
To ensure sufficient heating power, the supply voltage must be at least 24 V DC. Please also take into account a possible voltage drop on the cable between the power supply unit and the device.
Under certain conditions, the heating power may not be sufficient. Knowledge article no. KA-08821 already describes how the power of the internal heating can be increased for the DL100 distance sensors. The same applies to Dx500 with exception of the nominal heating power, which is 20 W @ 24V for Dx500.