Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
Why is the response time up to 200 % of the specification?
Article No: KA-10526
Version: 1.0
Subject to change without notice
Related Products
UM30-2
UC12
UC40
UC30
UM18-2 Core
UC4
UM12
Table of Contents
SICK does not define response time of analog output as the time until a visible reaction, but until 90% of the end value is reached.
This approximation of the final value depends on the settings of the average filter. For this reason, a footnote has been added to UC4, that the response time might be extended up to 200% in reference to the device specification.
Example:
With all analog variants, except UM18-2, the average filter is filled with max. distance values (=limiting range values) by default when switching on. Depending on the output scaling, a jump to a closer distance initially takes a certain amount of time before the calculated average value falls within the scaled window and a reaction can be seen on the analog output. The similar behaviour occurs when the sensor looks into infinity (= max. distance) and then an object enters sideways at a short distance.