web
You’re offline. This is a read only version of the page.
close
Support Portal

TMM88D energency message 0x5040

What is the meaning of the emercency message 0x5040 of the inclinationsensor TMS88D and TMM88D?
Related Products
TMS/TMM88 Dynamic

Table of Contents

The warning 0x5040 in the emergency message of the TMS88D and TMM88D CANopen devices is only an accuracy warning.

It indicates that the measured acceleration or angular rate values are outside the sensor's specified measurement range. As a result, the accuracy of the calculated inclination angle may be limited.

This warning can occur if the sensor is subjected to excessive movement or shock, causing the internal sensing element to operate outside its valid range. In such cases, the reported inclination value may deviate from the specified accuracy.

Keywords:
TMS88D,TMM88D, Emercency message