Your SICK ID gives you access to our extensive range of services. This includes direct online orders, price and availability checks, and access to our digital services.
How to interpret the AHS36 / AHM36 Serial Number from CANopen object 650Bh and 1018.4h?
Article No: KA-10524
Version: 1.0
Subject to change without notice
Related Products
AHS/AHM36
Table of Contents
Serial Number interpretation and differences between type label and CANopen objects
The serial number at AHS36 / AHM36 get visible at type label or is available via CANopen objects 650Bh and 1018.4h. But the serial number from type label (see picture below) and content of the object 650Bh (object 1018.4h is equal to 650Bh) are different displayed and additional the objects contains a type code as well.
Serial number on type label, for example 26020273, shows following information: 26 = Year 2026 02 = Calendar week 2 0273 = Counting number
Same encoder contains in the objects 650Bh / 1018.4h the serial number 0x231A0911 (588908817) which is different to 26020273. Next example shows how the serial number from the CANopen objects must be decoded to get the similar value like on the type label.