Rest assured, our magnetic sensors pose no risk when installed in close proximity to each other. Unlike inductive sensors, which require varying oscillation frequencies when mounted closely, our magnetic sensors do not generate an active field that could potentially interfere with each other.
The performance of our magnetic sensors is primarily influenced by the shape of the magnetic field of the magnet and any nearby ferromagnetic objects that could alter this field. These factors determine the switching behavior of the magnetic sensor. Therefore, it is essential to consider the placement of magnets and ferromagnetic objects when installing our magnetic sensors. Please feel free to reach out if you have any further questions or concerns. We are here to assist you.